SingleElementConveyorBuilder Class¶
-
class
NXOpen.LineDesigner.
SingleElementConveyorBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateSingleElementConveyorBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
FirstConveyingSurfaceCroner | Returns or sets the first conveying surface corner of conveyor |
KfObject | Returns the kf object |
MovingDirection | Returns or sets the moving direction of conveyor |
PointOnConveyingSurface | Returns or sets the point on surface of conveyor are return |
Reversible | Returns or sets the option to check whether conveyor is reversible |
SecondConveyingSurfaceCorner | Returns or sets the second conveying surface corner of conveyor |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FirstConveyingSurfaceCroner¶
-
SingleElementConveyorBuilder.
FirstConveyingSurfaceCroner
¶ Returns or sets the first conveying surface corner of conveyor
-------------------------------------
Getter Method
Signature
FirstConveyingSurfaceCroner
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
FirstConveyingSurfaceCroner
Parameters: firstConveyingSurfaceCroner ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
KfObject¶
-
SingleElementConveyorBuilder.
KfObject
¶ Returns the kf object
-------------------------------------
Getter Method
Signature
KfObject
Returns: Return type: NXOpen.KFObject
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
MovingDirection¶
-
SingleElementConveyorBuilder.
MovingDirection
¶ Returns or sets the moving direction of conveyor
-------------------------------------
Getter Method
Signature
MovingDirection
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
MovingDirection
Parameters: dirVector ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PointOnConveyingSurface¶
-
SingleElementConveyorBuilder.
PointOnConveyingSurface
¶ Returns or sets the point on surface of conveyor are return
-------------------------------------
Getter Method
Signature
PointOnConveyingSurface
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PointOnConveyingSurface
Parameters: pointOnConveyingSurface ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Reversible¶
-
SingleElementConveyorBuilder.
Reversible
¶ Returns or sets the option to check whether conveyor is reversible
-------------------------------------
Getter Method
Signature
Reversible
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
Reversible
Parameters: reversible (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SecondConveyingSurfaceCorner¶
-
SingleElementConveyorBuilder.
SecondConveyingSurfaceCorner
¶ Returns or sets the second conveying surface corner of conveyor
-------------------------------------
Getter Method
Signature
SecondConveyingSurfaceCorner
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SecondConveyingSurfaceCorner
Parameters: secondConveyingSurfaceCorner ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
SingleElementConveyorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.