ProductionUnitCreatorBuilder Class¶
-
class
NXOpen.LineDesigner.
ProductionUnitCreatorBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateProductionUnitCreatorBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ProductionUnitId | Returns or sets the production unit id |
ProductionUnitName | Returns or sets the production unit name |
ProductionUnitTypeString | Returns or sets the type of a production unit |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AssignId | The assign ID of production unit |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetProductionUnitDescription | The production unit description |
SetProductionUnitDescription | The production unit description is set |
SetProductionUnitParent | The production unit parent is set |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ProductionUnitId¶
-
ProductionUnitCreatorBuilder.
ProductionUnitId
¶ Returns or sets the production unit id
-------------------------------------
Getter Method
Signature
ProductionUnitId
Returns: Return type: str New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ProductionUnitId
Parameters: productionUnitId (str) – New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ProductionUnitName¶
-
ProductionUnitCreatorBuilder.
ProductionUnitName
¶ Returns or sets the production unit name
-------------------------------------
Getter Method
Signature
ProductionUnitName
Returns: Return type: str New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ProductionUnitName
Parameters: productionUnitName (str) – New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ProductionUnitTypeString¶
-
ProductionUnitCreatorBuilder.
ProductionUnitTypeString
¶ Returns or sets the type of a production unit
-------------------------------------
Getter Method
Signature
ProductionUnitTypeString
Returns: Return type: str New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ProductionUnitTypeString
Parameters: productionUnitType (str) – New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
AssignId¶
-
ProductionUnitCreatorBuilder.
AssignId
¶ The assign ID of production unit
Signature
AssignId()
New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
GetProductionUnitDescription¶
-
ProductionUnitCreatorBuilder.
GetProductionUnitDescription
¶ The production unit description
Signature
GetProductionUnitDescription()
Returns: Return type: list of str New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetProductionUnitDescription¶
-
ProductionUnitCreatorBuilder.
SetProductionUnitDescription
¶ The production unit description is set
Signature
SetProductionUnitDescription(productionUnitDescription)
Parameters: productionUnitDescription (list of str) – New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetProductionUnitParent¶
-
ProductionUnitCreatorBuilder.
SetProductionUnitParent
¶ The production unit parent is set
Signature
SetProductionUnitParent(parent)
Parameters: parent ( NXOpen.Assemblies.Partition
) –New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
ProductionUnitCreatorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.