PickRectanglePointsBuilder Class¶
-
class
NXOpen.LineDesigner.
PickRectanglePointsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Pick Rectangle Points
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreatePickRectanglePointsBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AllowRotation | Returns or sets the check for rotaion |
PointsSelection | Returns the points of selection are return |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ResetData | To reset rectangle data |
ResetWidthHeight | To reset rectangle width and height |
SetWidthHeight | To set rectangle width and height |
UpdateRecAngle | To update rectangle angle |
UpdateRecHeight | To update rectangle height |
UpdateRecWidth | To update rectangle width |
UpdateRectangle | To update rectangle points |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllowRotation¶
-
PickRectanglePointsBuilder.
AllowRotation
¶ Returns or sets the check for rotaion
-------------------------------------
Getter Method
Signature
AllowRotation
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
AllowRotation
Parameters: rotaion (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PointsSelection¶
-
PickRectanglePointsBuilder.
PointsSelection
¶ Returns the points of selection are return
-------------------------------------
Getter Method
Signature
PointsSelection
Returns: Return type: NXOpen.SelectPartList
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
ResetData¶
-
PickRectanglePointsBuilder.
ResetData
¶ To reset rectangle data
Signature
ResetData()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ResetWidthHeight¶
-
PickRectanglePointsBuilder.
ResetWidthHeight
¶ To reset rectangle width and height
Signature
ResetWidthHeight()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetWidthHeight¶
-
PickRectanglePointsBuilder.
SetWidthHeight
¶ To set rectangle width and height
Signature
SetWidthHeight(width, height)
Parameters: - width (float) –
- height (float) –
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRecAngle¶
-
PickRectanglePointsBuilder.
UpdateRecAngle
¶ To update rectangle angle
Signature
UpdateRecAngle(angle)
Parameters: angle (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRecHeight¶
-
PickRectanglePointsBuilder.
UpdateRecHeight
¶ To update rectangle height
Signature
UpdateRecHeight(height)
Parameters: height (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRecWidth¶
-
PickRectanglePointsBuilder.
UpdateRecWidth
¶ To update rectangle width
Signature
UpdateRecWidth(width)
Parameters: width (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRectangle¶
-
PickRectanglePointsBuilder.
UpdateRectangle
¶ To update rectangle points
Signature
UpdateRectangle()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
PickRectanglePointsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.