JigOnPlaneBuilder Class¶
-
class
NXOpen.LineDesigner.
JigOnPlaneBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Jig on plane
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateJigOnPlaneBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
SelectedPoints | Returns the selected points |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
GetJigPlaneParams | Selected jig plane matrix |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectedPoints¶
-
JigOnPlaneBuilder.
SelectedPoints
¶ Returns the selected points
-------------------------------------
Getter Method
Signature
SelectedPoints
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
GetJigPlaneParams¶
-
JigOnPlaneBuilder.
GetJigPlaneParams
¶ Selected jig plane matrix
Signature
GetJigPlaneParams()
Returns: a tuple Return type: A tuple consisting of (rotation, origin). rotation is a NXOpen.Matrix3x3
. origin is aNXOpen.Vector3d
.New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
JigOnPlaneBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.