GateFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
GateFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.GateFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateGateFeatureBuilder()
Default values.
Property Value LinearDimElevation.Value 650 (millimeters part), 25.6 (inches part) LinearDimGateThickness.Value 37.5 (millimeters part), 1.5 (inches part) OpeningStyleEnum Left New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
LinearDimElevation | Returns the elevation used for creation of gate |
LinearDimGateThickness | Returns the gate thickness |
OpeningStyleEnum | Returns or sets the opening style of gate |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GateFeatureBuilderGateOpeningStyle Enumeration | This enum represents gate opening style |
Property Detail¶
LinearDimElevation¶
-
GateFeatureBuilder.
LinearDimElevation
¶ Returns the elevation used for creation of gate
-------------------------------------
Getter Method
Signature
LinearDimElevation
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinearDimGateThickness¶
-
GateFeatureBuilder.
LinearDimGateThickness
¶ Returns the gate thickness
-------------------------------------
Getter Method
Signature
LinearDimGateThickness
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OpeningStyleEnum¶
-
GateFeatureBuilder.
OpeningStyleEnum
¶ Returns or sets the opening style of gate
-------------------------------------
Getter Method
Signature
OpeningStyleEnum
Returns: Return type: NXOpen.LineDesigner.GateFeatureBuilderGateOpeningStyle
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
OpeningStyleEnum
Parameters: openingStyleEnum ( NXOpen.LineDesigner.GateFeatureBuilderGateOpeningStyle
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
GateFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.