CreateFactoryElementBuilderTypeAPI Enumeration¶
NXOpen.LineDesigner.CreateFactoryElementBuilder.TypeAPI is an alias for NXOpen.LineDesigner.CreateFactoryElementBuilderTypeAPI
-
class
NXOpen.LineDesigner.
CreateFactoryElementBuilderTypeAPI
¶ Bases:
object
This enum is providing possible element types
Enum Members
Enum Member Enum Member Description Plant Represents the Plant type Station Represents the Station type Line Represents the Line type Zone Represents the Zone type Partition Represents the Partition type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-