ConnectionCreatorBuilder Class¶
-
class
NXOpen.LineDesigner.
ConnectionCreatorBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateConnectionCreatorBuilder()
Default values.
Property Value ConectionOffset.Value 0 (millimeters part), 0 (inches part) ConectionType MoveAndConnect New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConectionOffset | Returns the connection offset |
ConectionType | Returns or sets the current connection type |
SourceConnector | Returns the source connector used in connection |
Tag | Returns the Tag for this object. |
TargetConnector | Returns the target connector used in connection |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConnectionCreatorBuilderConnectionType Enumeration | This enum is providing possible connection types |
Property Detail¶
ConectionOffset¶
-
ConnectionCreatorBuilder.
ConectionOffset
¶ Returns the connection offset
-------------------------------------
Getter Method
Signature
ConectionOffset
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ConectionType¶
-
ConnectionCreatorBuilder.
ConectionType
¶ Returns or sets the current connection type
-------------------------------------
Getter Method
Signature
ConectionType
Returns: Return type: NXOpen.LineDesigner.ConnectionCreatorBuilderConnectionType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ConectionType
Parameters: conectionType ( NXOpen.LineDesigner.ConnectionCreatorBuilderConnectionType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SourceConnector¶
-
ConnectionCreatorBuilder.
SourceConnector
¶ Returns the source connector used in connection
-------------------------------------
Getter Method
Signature
SourceConnector
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TargetConnector¶
-
ConnectionCreatorBuilder.
TargetConnector
¶ Returns the target connector used in connection
-------------------------------------
Getter Method
Signature
TargetConnector
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
ConnectionCreatorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.