LightSceneType Enumeration¶
NXOpen.Light.SceneType is an alias for NXOpen.LightSceneType
-
class
NXOpen.
LightSceneType
¶ Bases:
object
The predefined scene lights used in Basic Lights. These are subtypes of
LightType.Scene
. Except for ambient light, all of the other lights are on the same side of the model as the observer.Enum Members
Enum Member Enum Member Description NotASceneLight The light is not a scene light Ambient Light from all around the model LeftTop Light from the top left of the view Top Light from the top center of the view RightTop Light from the top right of the view Front Light from the front of the view (at the observer’s location LeftBottom Light from the bottom left of the view Bottom Light from the bottom center of the view RightBottom Light from the bottom right of the view -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-