Constants Enumeration¶
-
class
NXOpen.Layer.
Constants
¶ Bases:
object
Constants for layers Enum Members
Enum Member Enum Member Description FirstLayer The number of the first layer. Valid layers are numbered from LayerConstants.FirstLayer
toLayerConstants.LastLayer
LastLayer The number of the last layer. Valid layers are numbered from LayerConstants.FirstLayer
toLayerConstants.LastLayer
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-