JtCreatorPmiOption Enumeration¶
NXOpen.JtCreator.PmiOption is an alias for NXOpen.JtCreatorPmiOption
-
class
NXOpen.
JtCreatorPmiOption
¶ Bases:
object
Include PMI options
Enum Members
Enum Member Enum Member Description NotSet NONE PartOnly PARTS_ONLY AsmOnly ASM_ONLY PartAndAsm PARTS_AND_ASM -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-