JamSession Class¶
-
class
NXOpen.
JamSession
¶ Bases:
NXOpen.TaggedObject
Represents a Jam session
No creator defined as this is an internal class
New in version NX3.0.2.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
Colors | used to manage the standard NX colors |
Methods¶
Method | Description |
---|---|
GetAllocationStatistics | Get the allocation statistics |
GetOMSchema | Returns a schema |
GetOMSchemas | Returns the schemas |
NewJamTest | Create new JamTest |
Structs¶
JamSessionAllocationStatistics_Struct Struct | Allocation statistics |
Method Detail¶
GetAllocationStatistics¶
-
JamSession.
GetAllocationStatistics
¶ Get the allocation statistics
Signature
GetAllocationStatistics()
Returns: Return type: NXOpen.JamSessionAllocationStatistics_Struct
New in version NX4.0.0.
License requirements: None.
GetOMSchema¶
-
JamSession.
GetOMSchema
¶ Returns a schema
Signature
GetOMSchema(name)
Parameters: name (str) – Returns: Return type: NXOpen.OMSchema
New in version NX4.0.0.
License requirements: None.
GetOMSchemas¶
-
JamSession.
GetOMSchemas
¶ Returns the schemas
Signature
GetOMSchemas()
Returns: Return type: list of NXOpen.OMSchema
New in version NX4.0.0.
License requirements: None.