ItemCacheMappedEntityBuilder Class¶
-
class
NXOpen.
ItemCacheMappedEntityBuilder
¶ Bases:
NXOpen.Builder
Generic journal methods for ItemCacheMappedEntityBuilder
Not support KF.
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ItemDescription | Returns or sets the description value. |
ItemId | Returns or sets the id value. |
ItemName | Returns or sets the name value. |
ItemPropertyTable | Returns the property table associated with the object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ItemDescription¶
-
ItemCacheMappedEntityBuilder.
ItemDescription
¶ Returns or sets the description value.
-------------------------------------
Getter Method
Signature
ItemDescription
Returns: Description value. Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemDescription
Parameters: description (str) – Description value. New in version NX12.0.0.
License requirements: None.
ItemId¶
-
ItemCacheMappedEntityBuilder.
ItemId
¶ Returns or sets the id value.
-------------------------------------
Getter Method
Signature
ItemId
Returns: The ID value. Return type: int New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemId
Parameters: id (int) – The ID value. New in version NX12.0.0.
License requirements: None.
ItemName¶
-
ItemCacheMappedEntityBuilder.
ItemName
¶ Returns or sets the name value.
-------------------------------------
Getter Method
Signature
ItemName
Returns: The name string value. Return type: str New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ItemName
Parameters: name (str) – The name string value. New in version NX12.0.0.
License requirements: None.
ItemPropertyTable¶
-
ItemCacheMappedEntityBuilder.
ItemPropertyTable
¶ Returns the property table associated with the object
-------------------------------------
Getter Method
Signature
ItemPropertyTable
Returns: property table Return type: NXOpen.CAE.PropertyTable
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ItemCacheMappedEntityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.