NXOpen.Issue Package

Classes

IssueAttachment Class Represents the Issue Attachment object.
IssueBriefcase Class Represents the Issue Briefcase object.
IssueBriefcaseSynchronizeBuilder Class Represents a NXOpen.Issue.IssueBriefcase synchronize builder
IssueContent Class Represents the Issue Issue object.
IssueContentBuilder Class Represents a NXOpen.Issue.IssueContent builder
IssueFolder Class Represents the Issue Folder object.
IssueList Class Represents the Issue List object.
IssueListCollection Class Represents a NXOpen.Issue.IssueListCollection
IssueManager Class Contains the collection objects for creating and iterating over issue objects.
IssueProperty Class Represents the Issue Property object.
IssueSite Class Represents the Issue Site object.
SnapshotSubsetBuilder Class Used to create or edit issue snapshot subset.
SnapshotWorksetBuilder Class Used to create or edit issue snapshot workset which is a container to hold all the corresponding parts to represent an issue.

Enumerations

IssueAttachmentType Enumeration Represents the possible attachment types for a NXOpen.Issue.IssueAttachment.
IssueFolderType Enumeration Represents the possible folder types for a NXOpen.Issue.IssueFolder.
IssueManagerMode Enumeration Represents the possible issue site modes.
IssueManagerState Enumeration Represents the possible issue object states.
IssuePropertyType Enumeration Represents the possible property types.
SnapshotSubsetBuilderContextType Enumeration The option specifying which kinds of issue snapshot subset should be created.