IssuePropertyType Enumeration¶
NXOpen.Issue.IssueProperty.Type is an alias for NXOpen.Issue.IssuePropertyType
-
class
NXOpen.Issue.
IssuePropertyType
¶ Bases:
object
Represents the possible property types. for a
NXOpen.Issue.IssueProperty
.Enum Members
Enum Member Enum Member Description Text Text type Note Note type User User type Choice Choice type Url URL type Boolean Boolean type Date Date type Number Number type Integer Integer type Point3D 3D point type Vector3D 3D vector type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-