IssueManagerState Enumeration¶
NXOpen.Issue.IssueManager.State is an alias for NXOpen.Issue.IssueManagerState
-
class
NXOpen.Issue.
IssueManagerState
¶ Bases:
object
Represents the possible issue object states.
Enum Members
Enum Member Enum Member Description Original Original state Created Created state Modified Modified state Removed Removed state -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-