IssueListCollection Class¶
-
class
NXOpen.Issue.
IssueListCollection
¶ Bases:
object
Represents a
NXOpen.Issue.IssueListCollection
To obtain an instance of this class, refer to
NXOpen.Issue.IssueManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Issue.IssueList with the given name. |
Method Detail¶
FindObject¶
-
IssueListCollection.
FindObject
¶ Finds the
NXOpen.Issue.IssueList
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Issue.IssueList
.Returns: NXOpen.Issue.IssueList
with this name.Return type: NXOpen.Issue.IssueList
New in version NX8.5.0.
License requirements: nx_issue_mgmt (“NX Issue Tracking”)