IssueFolderType Enumeration¶
NXOpen.Issue.IssueFolder.Type is an alias for NXOpen.Issue.IssueFolderType
-
class
NXOpen.Issue.
IssueFolderType
¶ Bases:
object
Represents the possible folder types for a
NXOpen.Issue.IssueFolder
.Enum Members
Enum Member Enum Member Description ProblemItems Problem items type ImpactedItems Impacted items type ReferenceItems Reference items type ImplementedBy Implemented by type IssueImage Issue image type IssueFixedImage Issue fixed image type SnapshotBeforeFix Snapshot before fix type SnapshotAfterFix Snapshot after fix type ValidationResults ValidationResult type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-