IssueAttachmentType Enumeration¶
NXOpen.Issue.IssueAttachment.Type is an alias for NXOpen.Issue.IssueAttachmentType
-
class
NXOpen.Issue.
IssueAttachmentType
¶ Bases:
object
Represents the possible attachment types for a
NXOpen.Issue.IssueAttachment
.Enum Members
Enum Member Enum Member Description Generic Generic type Text Text type Part Part type Xml XML type Image Image type ValidationLog Validation log file Bookmark Bookmark type Snapshot Snapshot type ValidationResult ValidationResult object type Workset Workset type ShapeDesignElement Shape Design Element type ReuseDesignElement Reuse Design Element type SubordinateDesignElement Subordinate Design Element type PromissoryDesignElement Promissory Design Element type DesignControlElement Design Control Element type Subset Subset type MSWord Microsoft Word type MSExcel Microsoft Excel type MSPowerPoint Microsoft Power Point type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-