HumanReachZoneMethodType Enumeration

NXOpen.HumanReachZone.MethodType is an alias for NXOpen.HumanReachZoneMethodType

class NXOpen.HumanReachZoneMethodType

Bases: object

This enum represents the methods for computing the reach zone

Enum Members

Enum Member Enum Member Description
ShoulderOnly
FlexWaist
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.