HumanPosturePredictionBuilderVehicleType Enumeration¶
NXOpen.HumanPosturePredictionBuilder.VehicleType is an alias for NXOpen.HumanPosturePredictionBuilderVehicleType
-
class
NXOpen.
HumanPosturePredictionBuilderVehicleType
¶ Bases:
object
Represents the vehicle type.
Enum Members
Enum Member Enum Member Description ClassA Indicate Class A vehicle. Vehicles with H-point heights (H30) less than 405 mm and steering wheel diameters (W9) less than 450 mm. This class of vehicles includes passenger cars, multipurpose passenger vehicles, and vans. ClassB Indicate Class B vehicle. Vehicles with H-point heights (H30) between 405 and 530 mm and steering wheel diameters (W9) between 450 and 560 mm with treadle accelerator pedals. This class of vehicles includes heavy trucks, some medium duty trucks, and some buses. ClassSeatedSoldier Seated soldier -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-