HumanHandsDialogBuilderDatabaseType Enumeration¶
NXOpen.HumanHandsDialogBuilder.DatabaseType is an alias for NXOpen.HumanHandsDialogBuilderDatabaseType
-
class
NXOpen.
HumanHandsDialogBuilderDatabaseType
¶ Bases:
object
database used for scaling. likely to be dynamically generated at runtime
Enum Members
Enum Member Enum Member Description Ansur Ansur2 Nhanes Nhanes2014 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-