HumanHandShapeDataHandOpt Enumeration

NXOpen.HumanHandShapeData.HandOpt is an alias for NXOpen.HumanHandShapeDataHandOpt

class NXOpen.HumanHandShapeDataHandOpt

Bases: object

This enum represents the hand shape data type of human

Enum Members

Enum Member Enum Member Description
Left
Right
Both
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.