HumanDataWeightType Enumeration¶
NXOpen.HumanData.WeightType is an alias for NXOpen.HumanDataWeightType
-
class
NXOpen.
HumanDataWeightType
¶ Bases:
object
This enum represents the weight data type of human
Enum Members
Enum Member Enum Member Description Percentile99 Indicate weight is 99% of population Percentile95 Indicate weight is 95% of population Percentile50 Indicate weight is 50% of population Percentile5 Indicate weight is 5% of population Percentile1 Indicate weight is 1% of population Custom Indicate weight value is the actual weight of the human Regress Indicate weight value is computed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-