HumanDataSideType Enumeration¶
NXOpen.HumanData.SideType is an alias for NXOpen.HumanDataSideType
-
class
NXOpen.
HumanDataSideType
¶ Bases:
object
This enum represents the types of human side
Enum Members
Enum Member Enum Member Description Left Indicate the left side of human Right Indicate the right side of human Center Indicate the center of human -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-