HumanDataSegmentScalingType Enumeration¶
NXOpen.HumanData.SegmentScalingType is an alias for NXOpen.HumanDataSegmentScalingType
-
class
NXOpen.
HumanDataSegmentScalingType
¶ Bases:
object
This enum represents the types of the segment scaling variable names
Enum Members
Enum Member Enum Member Description Head Indicate scaling of head Neck Indicate scaling of neck Torso Indicate scaling of torso UpperArm Indicate scaling of upper_arm LowerArm Indicate scaling of lower_arm Hand Indicate scaling of hand LowerTorso Indicate scaling of lower_torso UpperLeg Indicate scaling of upper_leg LowerLeg Indicate scaling of lower_leg Foot Indicate scaling of foot -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-