HumanDataReferencePointType Enumeration¶
NXOpen.HumanData.ReferencePointType is an alias for NXOpen.HumanDataReferencePointType
-
class
NXOpen.
HumanDataReferencePointType
¶ Bases:
object
This enum represents the location of the reference point
Enum Members
Enum Member Enum Member Description No Indicate no reference point LeftEye Indicate reference point at the left eye RightEye Indicate reference point at the right eye HPoint Indicate reference point at the H-point LeftToe Indicate reference point at the left toe RightToe Indicate reference point at the right toe NumberReferences Indicate the number of reference point types -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-