HumanDataJointType Enumeration¶
NXOpen.HumanData.JointType is an alias for NXOpen.HumanDataJointType
-
class
NXOpen.
HumanDataJointType
¶ Bases:
object
This enum represents the types of the joint names
Enum Members
Enum Member Enum Member Description BaseOfNeck Indicate joint named base_of_neck LeftShoulder Indicate joint named left_shoulder RightShoulder Indicate joint named right_shoulder Torso Indicate joint named torso LeftElbow Indicate joint named left_elbow RightElbow Indicate joint named right_elbow LeftWrist Indicate joint named left_wrist RightWrist Indicate joint named right_wrist Lthumb0 Indicate joint named lthumb0 Lthumb1 Indicate joint named lthumb1 Lthumb2 Indicate joint named lthumb2 LeftFinger00 Indicate joint named left_finger00 Linfinger01 Indicate joint named linfinger01 Linfinger02 Indicate joint named linfinger02 LeftFinger10 Indicate joint named left_finger10 Lmidfinger11 Indicate joint named lmidfinger11 Lmidfinger12 Indicate joint named lmidfinger12 LeftFinger20 Indicate joint named left_finger20 Lringfinger21 Indicate joint named lringfinger21 Lringfinger22 Indicate joint named lringfinger22 LeftFinger30 Indicate joint named left_finger30 Lpinfinger31 Indicate joint named lpinfinger31 Lpinfinger32 Indicate joint named lpinfinger32 Rthumb0 Indicate joint named rthumb0 Rthumb1 Indicate joint named rthumb1 Rthumb2 Indicate joint named rthumb2 RightFinger00 Indicate joint named right_finger00 Rinfinger01 Indicate joint named rinfinger01 Rinfinger02 Indicate joint named rinfinger02 RightFinger10 Indicate joint named right_finger10 Rmidfinger11 Indicate joint named rmidfinger11 Rmidfinger12 Indicate joint named rmidfinger12 RightFinger20 Indicate joint named right_finger20 Rringfinger21 Indicate joint named rringfinger21 Rringfinger22 Indicate joint named rringfinger22 RightFinger30 Indicate joint named right_finger30 Rpinfinger31 Indicate joint named rpinfinger31 Rpinfinger32 Indicate joint named rpinfinger32 Waist Indicate joint named waist LeftHip Indicate joint named left_hip RightHip Indicate joint named right_hip LeftKnee Indicate joint named left_knee RightKnee Indicate joint named right_knee LeftAnkle Indicate joint named left_ankle RightAnkle Indicate joint named right_ankle LeftToes Indicate joint named left_toes RightToes Indicate joint named right_toes -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-