HumanDataInverseKinematicsInitJoint Enumeration¶
NXOpen.HumanData.InverseKinematicsInitJoint is an alias for NXOpen.HumanDataInverseKinematicsInitJoint
-
class
NXOpen.
HumanDataInverseKinematicsInitJoint
¶ Bases:
object
This enum represents the motion initiation joint of hand dynamic drag
Enum Members
Enum Member Enum Member Description Shoulder Indicate starting at the shoulder for simple arm motions without changing the upper body position. Waist Indicate starting arm motion at the waist and using the entire upper body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-