HumanDataInverseKinematicsBalanceType Enumeration¶
NXOpen.HumanData.InverseKinematicsBalanceType is an alias for NXOpen.HumanDataInverseKinematicsBalanceType
-
class
NXOpen.
HumanDataInverseKinematicsBalanceType
¶ Bases:
object
This enum represents the balance type of active reach
Enum Members
Enum Member Enum Member Description AllowStep Indicate human is allowed to move one step to keep balance NoStep Indicate human foot is fixate without step KeepSeated Indicate human is in a seated position and thus supported by the lower torso -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-