HumanDataHandGoalType Enumeration¶
NXOpen.HumanData.HandGoalType is an alias for NXOpen.HumanDataHandGoalType
-
class
NXOpen.
HumanDataHandGoalType
¶ Bases:
object
This enum represents the type to define hand goal position
Enum Members
Enum Member Enum Member Description GoalPoint Indicate the hand goal is point GoalCsys Indicate the hand goal is csys HandFigure Indicate the hand goal is hand figure -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-