HumanDataEditDisplayBodyParts Enumeration¶
NXOpen.HumanData.EditDisplayBodyParts is an alias for NXOpen.HumanDataEditDisplayBodyParts
-
class
NXOpen.
HumanDataEditDisplayBodyParts
¶ Bases:
object
This enum represents the body parts of edit human display
Enum Members
Enum Member Enum Member Description LeftEyePoint Indicate edit display body parts named left eye point RightEyePoint Indicate edit display body parts named right eye point MidEyePoint Indicate edit display body parts named mid eye point HipPoint Indicate edit display body parts named hip point LeftToePoint Indicate edit display body parts named left toe point RightToePoint Indicate edit display body parts named right toe point LeftHeelPoint Indicate edit display body parts named left heel point RightHeelPoint Indicate edit display body parts named right heel point CenterOfMass Indicate edit display body parts named center of mass All Indicate edit display body parts named all -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-