TrimCurveBoundingObjectBuilder Class¶
-
class
NXOpen.GeometricUtilities.
TrimCurveBoundingObjectBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.GeometricUtilities.TrimCurveBoundingObjectBuilder
To create a new instance of this class, use
NXOpen.Features.TrimCurve2Builder.CreateTrimCurveBoundingObjectBuilder()
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
BoundingObject | Returns the bounding object |
BoundingObjectList | Returns the bounding object list Only one object is allowed in this list. |
BoundingObjectMethodType | Returns or sets the bounding object enum type |
BoundingPlane | Returns or sets the bounding plane |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TrimCurveBoundingObjectBuilderMethod Enumeration | the Object or Plane selection |
Property Detail¶
BoundingObject¶
-
TrimCurveBoundingObjectBuilder.
BoundingObject
¶ Returns the bounding object
-------------------------------------
Getter Method
Signature
BoundingObject
Returns: Get bounding object Return type: NXOpen.SelectDisplayableObject
New in version NX11.0.1.
Deprecated since version NX12.0.0: Use
NXOpen.GeometricUtilities.TrimCurveBoundingObjectBuilder.BoundingObjectList()
.License requirements: None.
BoundingObjectList¶
-
TrimCurveBoundingObjectBuilder.
BoundingObjectList
¶ Returns the bounding object list
Only one object is allowed in this list.
In the case of multiple objects, only first object will be considered for the operation.
-------------------------------------
Getter Method
Signature
BoundingObjectList
Returns: Get bounding object list Return type: NXOpen.SelectDisplayableObjectList
New in version NX12.0.0.
License requirements: None.
BoundingObjectMethodType¶
-
TrimCurveBoundingObjectBuilder.
BoundingObjectMethodType
¶ Returns or sets the bounding object enum type
-------------------------------------
Getter Method
Signature
BoundingObjectMethodType
Returns: Set bounding object type Return type: NXOpen.GeometricUtilities.TrimCurveBoundingObjectBuilderMethod
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingObjectMethodType
Parameters: boundingObjectMethod ( NXOpen.GeometricUtilities.TrimCurveBoundingObjectBuilderMethod
) – Set bounding objectNew in version NX11.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
BoundingPlane¶
-
TrimCurveBoundingObjectBuilder.
BoundingPlane
¶ Returns or sets the bounding plane
-------------------------------------
Getter Method
Signature
BoundingPlane
Returns: Set bounding plane object tag Return type: NXOpen.Plane
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingPlane
Parameters: plane ( NXOpen.Plane
) – Set bounding plane object tagNew in version NX11.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)