TransitionCurveBuilderTangentDirections Enumeration¶
NXOpen.GeometricUtilities.TransitionCurveBuilder.TangentDirections is an alias for NXOpen.GeometricUtilities.TransitionCurveBuilderTangentDirections
-
class
NXOpen.GeometricUtilities.
TransitionCurveBuilderTangentDirections
¶ Bases:
object
Tangent direction options
Enum Members
Enum Member Enum Member Description Rail transition curve will be tangent to the blend rail curve Limit transition curve will be tangent to the limit curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-