TransformerDataObjectType Enumeration

NXOpen.GeometricUtilities.TransformerData.ObjectType is an alias for NXOpen.GeometricUtilities.TransformerDataObjectType

class NXOpen.GeometricUtilities.TransformerDataObjectType

Bases: object

Type of objects.

Enum Members

Enum Member Enum Member Description
NotSet
Origin
TranslationX
TranslationY
TranslationZ
RotationXY
RotationYZ
RotationXZ
ScaleX
ScaleY
ScaleZ
DirectionX
DirectionY
DirectionZ
PlaneXY
PlaneYZ
PlaneXZ
ArcXY
ArcYZ
ArcXZ
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.