StepOptionBehavior Class¶
-
class
NXOpen.GeometricUtilities.
StepOptionBehavior
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.StepOptionBehavior
It provides several step options for controlling behavior when move face and so on.New in version NX8.0.1.
Properties¶
Property | Description |
---|---|
StepOption | Returns or sets the step option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StepOptionBehaviorStepOptionType Enumeration | Step Faec options |
Property Detail¶
StepOption¶
-
StepOptionBehavior.
StepOption
¶ Returns or sets the step option
-------------------------------------
Getter Method
Signature
StepOption
Returns: Return type: NXOpen.GeometricUtilities.StepOptionBehaviorStepOptionType
New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepOption
Parameters: stepOption ( NXOpen.GeometricUtilities.StepOptionBehaviorStepOptionType
) –New in version NX8.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
StepOptionBehavior.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.