StartHoleDataHoleForms Enumeration¶
NXOpen.GeometricUtilities.StartHoleData.HoleForms is an alias for NXOpen.GeometricUtilities.StartHoleDataHoleForms
-
class
NXOpen.GeometricUtilities.
StartHoleDataHoleForms
¶ Bases:
object
This enum represents hole form options in start plate of hole series.
Enum Members
Enum Member Enum Member Description Simple Simple hole form Counterbored Counterbored hole form Countersink Countersink hole form -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-