SplineExtensionBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SplineExtensionBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Spline extension builder class.
This class allows natural extension or trimming of a b-spline cuve. .. versionadded:: NX8.0.0
Properties¶
Property | Description |
---|---|
EndExtensionOption | Returns or sets the extension options |
EndPoint | Returns or sets the point up to which end is extended |
EndValue | Returns the end value |
IsSymmetric | Returns or sets the flag indicating if extension is symmetry. |
StartExtensionOption | Returns or sets the extension options |
StartPoint | Returns or sets the point up to which start is extended |
StartValue | Returns the start value |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SplineExtensionBuilderExtensionOption Enumeration | Spline extension options |
Property Detail¶
EndExtensionOption¶
-
SplineExtensionBuilder.
EndExtensionOption
¶ Returns or sets the extension options
-------------------------------------
Getter Method
Signature
EndExtensionOption
Returns: Return type: NXOpen.GeometricUtilities.SplineExtensionBuilderExtensionOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndExtensionOption
Parameters: extensionOption ( NXOpen.GeometricUtilities.SplineExtensionBuilderExtensionOption
) –New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
EndPoint¶
-
SplineExtensionBuilder.
EndPoint
¶ Returns or sets the point up to which end is extended
-------------------------------------
Getter Method
Signature
EndPoint
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPoint
Parameters: endPoint ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
EndValue¶
-
SplineExtensionBuilder.
EndValue
¶ Returns the end value
-------------------------------------
Getter Method
Signature
EndValue
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
IsSymmetric¶
-
SplineExtensionBuilder.
IsSymmetric
¶ Returns or sets the flag indicating if extension is symmetry.
Symmetric extension follows start extension values
-------------------------------------
Getter Method
Signature
IsSymmetric
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsSymmetric
Parameters: isSymmetric (bool) – New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
StartExtensionOption¶
-
SplineExtensionBuilder.
StartExtensionOption
¶ Returns or sets the extension options
-------------------------------------
Getter Method
Signature
StartExtensionOption
Returns: Return type: NXOpen.GeometricUtilities.SplineExtensionBuilderExtensionOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartExtensionOption
Parameters: extensionOption ( NXOpen.GeometricUtilities.SplineExtensionBuilderExtensionOption
) –New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
StartPoint¶
-
SplineExtensionBuilder.
StartPoint
¶ Returns or sets the point up to which start is extended
-------------------------------------
Getter Method
Signature
StartPoint
Returns: Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint
Parameters: startPoint ( NXOpen.Point
) –New in version NX8.0.0.
License requirements: features_modeling (“FEATURES MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
StartValue¶
-
SplineExtensionBuilder.
StartValue
¶ Returns the start value
-------------------------------------
Getter Method
Signature
StartValue
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SplineExtensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.