SpiralPatternSpiralDefineSize Enumeration¶
NXOpen.GeometricUtilities.SpiralPattern.SpiralDefineSize is an alias for NXOpen.GeometricUtilities.SpiralPatternSpiralDefineSize
-
class
NXOpen.GeometricUtilities.
SpiralPatternSpiralDefineSize
¶ Bases:
object
This defines size spiral type
Enum Members
Enum Member Enum Member Description NumberOfTurns using number of turns to define size of spiral TotalAngle using total angle to define size of spiral -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-