SpinePointDataCollection Class

class NXOpen.GeometricUtilities.SpinePointDataCollection

Bases: object

This class contains the factory methods for creating a SpinePointData object.

To obtain an instance of this class, refer to NXOpen.Part

New in version NX5.0.0.

Methods

Method Description
CreateSpinePointData Creates a SpinePointData object.

Method Detail

CreateSpinePointData

SpinePointDataCollection.CreateSpinePointData

Overloaded method CreateSpinePointData

  • CreateSpinePointData(lawValue, parameter, parent)
  • CreateSpinePointData(lawValueExpression, parameter, parent)

-------------------------------------

Creates a SpinePointData object.

Signature CreateSpinePointData(lawValue, parameter, parent)

Parameters:
  • lawValue (float) – Law value
  • parameter (float) – Parameter on path
  • parent (NXOpen.Section) – Section Curve on which projected point lies
Returns:

SpinePointData Object

Return type:

NXOpen.GeometricUtilities.SpinePointData

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)

-------------------------------------

Creates a SpinePointData object with expression.

Signature CreateSpinePointData(lawValueExpression, parameter, parent)

Parameters:
  • lawValueExpression (NXOpen.Expression) – Law value exp
  • parameter (float) – Parameter on path
  • parent (NXOpen.Section) – Section Curve on which projected point lies
Returns:

SpinePointData Object

Return type:

NXOpen.GeometricUtilities.SpinePointData

New in version NX5.0.0.

License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)

-------------------------------------