SpinePlaneBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SpinePlaneBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.GeometricUtilities.SpinePlaneBuilder
.To create a new instance of this class, use
NXOpen.Part.CreateEmptySpinePlaneBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Plane | Returns or sets the plane |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AlternateSolution | Creates the longer arc between the current and previous plane. |
Property Detail¶
Plane¶
-
SpinePlaneBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.Plane
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.Plane
) –New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)