SelectDividingObjectBuilder Class¶
-
class
NXOpen.GeometricUtilities.
SelectDividingObjectBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents the dividing tool block for dividing face
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ConstraintManager | Returns the iso parameter point |
CurvesToOffset | Returns the curves to offset |
DividingObjectsList | Returns the dividing objects list |
EndPoint | Returns or sets the end point |
IsoparametricDirection | Returns or sets the isoparametric direction |
OffsetDirection | Returns or sets the offset direction |
OffsetDistance | Returns the offset distance |
StartPoint | Returns or sets the start point |
Tag | Returns the Tag for this object. |
ToolOption | Returns or sets the tool option |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SelectDividingObjectBuilderIsoparametricDirectionType Enumeration | Represents the direction of isoparametric curve |
SelectDividingObjectBuilderToolType Enumeration | Represents the Dividing Tool types |
Property Detail¶
ConstraintManager¶
-
SelectDividingObjectBuilder.
ConstraintManager
¶ Returns the iso parameter point
-------------------------------------
Getter Method
Signature
ConstraintManager
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX9.0.0.
License requirements: None.
CurvesToOffset¶
-
SelectDividingObjectBuilder.
CurvesToOffset
¶ Returns the curves to offset
-------------------------------------
Getter Method
Signature
CurvesToOffset
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: None.
DividingObjectsList¶
-
SelectDividingObjectBuilder.
DividingObjectsList
¶ Returns the dividing objects list
-------------------------------------
Getter Method
Signature
DividingObjectsList
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX9.0.0.
License requirements: None.
EndPoint¶
-
SelectDividingObjectBuilder.
EndPoint
¶ Returns or sets the end point
-------------------------------------
Getter Method
Signature
EndPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPoint
Parameters: endPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
IsoparametricDirection¶
-
SelectDividingObjectBuilder.
IsoparametricDirection
¶ Returns or sets the isoparametric direction
-------------------------------------
Getter Method
Signature
IsoparametricDirection
Returns: Return type: NXOpen.GeometricUtilities.SelectDividingObjectBuilderIsoparametricDirectionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsoparametricDirection
Parameters: isoprametricDirection ( NXOpen.GeometricUtilities.SelectDividingObjectBuilderIsoparametricDirectionType
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
OffsetDirection¶
-
SelectDividingObjectBuilder.
OffsetDirection
¶ Returns or sets the offset direction
-------------------------------------
Getter Method
Signature
OffsetDirection
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetDirection
Parameters: offsetDirection (bool) – New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
OffsetDistance¶
-
SelectDividingObjectBuilder.
OffsetDistance
¶ Returns the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
StartPoint¶
-
SelectDividingObjectBuilder.
StartPoint
¶ Returns or sets the start point
-------------------------------------
Getter Method
Signature
StartPoint
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint
Parameters: startPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ToolOption¶
-
SelectDividingObjectBuilder.
ToolOption
¶ Returns or sets the tool option
-------------------------------------
Getter Method
Signature
ToolOption
Returns: Return type: NXOpen.GeometricUtilities.SelectDividingObjectBuilderToolType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolOption
Parameters: toolOption ( NXOpen.GeometricUtilities.SelectDividingObjectBuilderToolType
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
SelectDividingObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.