RefitControlBuilder Class¶
-
class
NXOpen.GeometricUtilities.
RefitControlBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
This class is used to specify the parameter set to refit faces
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DegreesAndSegmentsOrPatches | Returns the refit degrees and segments or patches |
RefitDirection | Returns or sets the refit direction |
RefitMethod | Returns or sets the refit method |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RefitControlBuilderRefitControlDirection Enumeration | Refit direction |
RefitControlBuilderRefitControlMethod Enumeration | Refit method |
Property Detail¶
DegreesAndSegmentsOrPatches¶
-
RefitControlBuilder.
DegreesAndSegmentsOrPatches
¶ Returns the refit degrees and segments or patches
-------------------------------------
Getter Method
Signature
DegreesAndSegmentsOrPatches
Returns: Return type: NXOpen.GeometricUtilities.DegreesAndSegmentsOrPatchesBuilder
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RefitDirection¶
-
RefitControlBuilder.
RefitDirection
¶ Returns or sets the refit direction
-------------------------------------
Getter Method
Signature
RefitDirection
Returns: Return type: NXOpen.GeometricUtilities.RefitControlBuilderRefitControlDirection
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
RefitDirection
Parameters: refitDirection ( NXOpen.GeometricUtilities.RefitControlBuilderRefitControlDirection
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RefitMethod¶
-
RefitControlBuilder.
RefitMethod
¶ Returns or sets the refit method
-------------------------------------
Getter Method
Signature
RefitMethod
Returns: Return type: NXOpen.GeometricUtilities.RefitControlBuilderRefitControlMethod
New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
RefitMethod
Parameters: refitMethod ( NXOpen.GeometricUtilities.RefitControlBuilderRefitControlMethod
) –New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Tolerance¶
-
RefitControlBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX6.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
Validate¶
-
RefitControlBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.