ReferencePattern Class¶
-
class
NXOpen.GeometricUtilities.
ReferencePattern
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
the reference pattern definition.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ReferencedPattern | Returns the referenced pattern object. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ResetBaseInstance | Reset the base instance indices to an undefined state. |
SetBaseInstance | Set the base instance |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ReferencedPattern¶
-
ReferencePattern.
ReferencedPattern
¶ Returns the referenced pattern object.
-------------------------------------
Getter Method
Signature
ReferencedPattern
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.0.0.
License requirements: None.
Method Detail¶
ResetBaseInstance¶
-
ReferencePattern.
ResetBaseInstance
¶ Reset the base instance indices to an “undefined” state.
The base instance will be reset so that the indices do not correspond to indices from any instance of the referenced pattern selected. The base instance indices must be set after this call before commit.
Signature
ResetBaseInstance()
New in version NX8.0.0.
License requirements: None.
SetBaseInstance¶
-
ReferencePattern.
SetBaseInstance
¶ Set the base instance
Signature
SetBaseInstance(firstIndex, secondIndex)
Parameters: - firstIndex (int) –
- secondIndex (int) –
New in version NX8.0.0.
License requirements: None.
Validate¶
-
ReferencePattern.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.