ReduceSurfaceRadiusBuilderReduceValueTypeSpecification Enumeration¶
NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilder.ReduceValueTypeSpecification is an alias for NXOpen.GeometricUtilities.ReduceSurfaceRadiusBuilderReduceValueTypeSpecification
-
class
NXOpen.GeometricUtilities.
ReduceSurfaceRadiusBuilderReduceValueTypeSpecification
¶ Bases:
object
Specify the reduction method. There are three types: percentage reduction, reduction value and target value.
Enum Members
Enum Member Enum Member Description Percentage Value Delta -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-