RectangularFrameBuilderAnchorLocationType Enumeration¶
NXOpen.GeometricUtilities.RectangularFrameBuilder.AnchorLocationType is an alias for NXOpen.GeometricUtilities.RectangularFrameBuilderAnchorLocationType
-
class
NXOpen.GeometricUtilities.
RectangularFrameBuilderAnchorLocationType
¶ Bases:
object
Anchor location types
Enum Members
Enum Member Enum Member Description TopLeft Top left position TopCenter Top center position TopRight Top right position MiddleLeft Middle left position MiddleCenter Middle center position MiddleRight Middle right position BottomLeft Bottom left position BottomCenter Bottom center position BottomRight Bottom right position -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-