PointsFromFileBuilder Class¶
-
class
NXOpen.GeometricUtilities.
PointsFromFileBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricUtilities.PointsFromFileBuilder
builder read points from a text file with format *.To create a new instance of this class, use
NXOpen.Part.CreatePointsFromFileBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CoordinateOption | Returns or sets the option indicating type of point coordinates |
FileName | Returns or sets the file name of the point data file |
PathName | Returns or sets the path name of the point data file |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PointsFromFileBuilderOptions Enumeration | Coordinate option |
Property Detail¶
CoordinateOption¶
-
PointsFromFileBuilder.
CoordinateOption
¶ Returns or sets the option indicating type of point coordinates
-------------------------------------
Getter Method
Signature
CoordinateOption
Returns: Return type: NXOpen.GeometricUtilities.PointsFromFileBuilderOptions
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoordinateOption
Parameters: option ( NXOpen.GeometricUtilities.PointsFromFileBuilderOptions
) –New in version NX8.5.0.
License requirements: None.
FileName¶
-
PointsFromFileBuilder.
FileName
¶ Returns or sets the file name of the point data file
-------------------------------------
Getter Method
Signature
FileName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FileName
Parameters: filename (str) – New in version NX8.5.0.
License requirements: None.
PathName¶
-
PointsFromFileBuilder.
PathName
¶ Returns or sets the path name of the point data file
-------------------------------------
Getter Method
Signature
PathName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PathName
Parameters: pathname (str) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
PointsFromFileBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.