PlayButtonsBuilderPlayModeValues Enumeration

NXOpen.GeometricUtilities.PlayButtonsBuilder.PlayModeValues is an alias for NXOpen.GeometricUtilities.PlayButtonsBuilderPlayModeValues

class NXOpen.GeometricUtilities.PlayButtonsBuilderPlayModeValues

Bases: object

the different play modes available

Enum Members

Enum Member Enum Member Description
PlayOnce
LoopOver
Retrace
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.