PatternSpacingSpacingType Enumeration¶
NXOpen.GeometricUtilities.PatternSpacing.SpacingType is an alias for NXOpen.GeometricUtilities.PatternSpacingSpacingType
-
class
NXOpen.GeometricUtilities.
PatternSpacingSpacingType
¶ Bases:
object
defines the type of spacing instances can have within a pattern.
Enum Members
Enum Member Enum Member Description Offset Specify distance from the origin of one instance to the origin of the next instance. Span Specify a distance for which all instances should occupy. PitchAndSpan Specify distance between instances and distance for all instances, number of copies is calculated. Pitch This is for pattern fill case. Count is calculated based on the pitch and fill boundary box. List Specify offsets with a list. PolygonCountPerSide This is for Polygon type. Specify number of count per side. PolygonPitchAlongSide This is for Polygon type. Specify a pitch distance along one side. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-