PatternOrientationProjDirEnum Enumeration¶
NXOpen.GeometricUtilities.PatternOrientation.ProjDirEnum is an alias for NXOpen.GeometricUtilities.PatternOrientationProjDirEnum
-
class
NXOpen.GeometricUtilities.
PatternOrientationProjDirEnum
¶ Bases:
object
pattern follow face project direction options available.
Enum Members
Enum Member Enum Member Description PatternPlaneNormal use pattern plane normal as project direction. NormalToFace project along face normal. RadialDir project along radial direction. This is specific for Circular pattern type. UserDefinedVector project along user defined vector. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-