PatternDefinitionPatternEnum Enumeration¶
NXOpen.GeometricUtilities.PatternDefinition.PatternEnum is an alias for NXOpen.GeometricUtilities.PatternDefinitionPatternEnum
-
class
NXOpen.GeometricUtilities.
PatternDefinitionPatternEnum
¶ Bases:
object
pattern types available. For details on the interface of each type, visit the corresponding definition class for each type.
Enum Members
Enum Member Enum Member Description Linear pattern along single linear direction. Circular pattern in angular and radial directions. Polygon polygon pattern. Spiral spiral pattern. AlongPath pattern along a section path. General general pattern. Reference reference pattern. Mirror mirror pattern. Helix helix pattern. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-